Part Number: LM5190-Q1 Other Parts Discussed in Thread: LM5190 Hello TI team,
I am working on a design with 48 V input and output of 5 V at 3.5 A using LM5190-Q1. However, I could not find any formulas or calculation guidelines in the LM5190‑Q1 datasheet…
Part Number: LM5190-Q1 Other Parts Discussed in Thread: TINA-TI Hello there.
chi-nguyen@ti.com
Could you please share the LM5190-Q1 spice model for simulation?
Thank you!
Part Number: LM5190-Q1 Other Parts Discussed in Thread: LM5190 I did a design based the LM5190 EVM and neither the EVM or my design can transition correctly into Constant-Current (CC) mode at 8A or above. Instead, both designs at max Iout begin modulating…
Part Number: LM5190-Q1 Other Parts Discussed in Thread: LM5190 Hello,
We're considering the LM5190 for a design. Do y'all have recommendations or guidelines on how to interleave n>=2 of these ICs? I.e. by doing the following for n=2:
Setting FB…
Part Number: LM5190-Q1 ’ve been working on the design of the LM5190-Q1 to meet the ±1V variation during transient behavior. I used the values suggested by the Quick Start Calculator Excel sheet, but I’m not able to achieve the specified requirement. I…
Part Number: LM5190-Q1 Dear TI team,
We are developing a 48V to 12V, 1.5A with LM5190-Q1 buck controller. Please find the specifications below:
Vin: 30 to 60V
Vout: 12V @ 1.5A
Switching frequency chosen: 112kHz
Inductor chosen: 220uH (74437529203221…
Part Number: LM5190-Q1 Hi TI team,
For my design, the input voltage is 48 V and the output voltage is 5 V at 3.5 A. For this application, I intend to operate the device at a switching frequency of 112 kHz. Kindly let me know whether this switching…
Part Number: LM5190-Q1 Other Parts Discussed in Thread: LM5190 Hi Sir,
My customer will use the LM5190-Q1 for the following design specifications: • Vin: 9~60V • Vout: 9V • Iout: 10A • fsw: 400kHz
Could you please help us verify the following key…
Part Number: LM5190-Q1 Other Parts Discussed in Thread: LM5190 , I need Ti to perform a design review of my implemenatio of the LM5190 . For this I can provide the schematics and a Qucikstart file. Do you need anything else?
Also I have an active NDA…