Part Number: LM53600-Q1 Support Path: /Product/Production, ordering, and quality/Product lifetime considerations/ I am looking at designing in a DC-DC buck converter. The LM53600-Q1 seems to fit all of my requirements, but I am concerned with product…
Part Number: LM53600-Q1 Tool/software: WEBENCH® Design Tools Hello Team,
I have a question about how to use Webench.
How do I change to FPWM mode?
Best regards,
Kato
Hi Glen ,
You can sync the LM53600-Q1 at 1.6MHz .
The reason for not allowing a wide sync frequency is the fact that the slope comp as well as loop comp is optimized for above AM band operation .
The frequency shift at higher input voltage is intended…
Other Parts Discussed in Thread: LM53600-Q1 Hello,
the new LM53600-Q1 seems to fit all my needs as a power supply for a hand held pressure measuring instrument. I have a question regarding the the Vcc pin of this device: Is the Vcc voltage available…
Hello all, I have two questions.
Q1. How many is the efficiency of Iout=100uA? Input Voltage is 8V,13.5V, 18V and 36V Mode = Auto 3.3V Fix Output
Q2. How many is the maximum value of High side MOSFET Rdson
Regards,
Koji Hayashi
Hi Team,
Our customer needs to the following spec.
Therefore, we would like to know the official parts number of TPS53600-Q1.
[Customer’s request spec]
-Output voltage is 650mA
-Output voltage 3.3V fixed
-With Spread Spectrum
I refer…
Hello Matsumoto-san,
We apologize for the delay.
The LM53600-Q1 does have true forced PWM mode but only works with standard BOM with an output voltage range of 3.3 V to 6 V. If your output voltage is in this range, the LM53600-Q1 does exactly what…
Part Number: ADS124S08 Other Parts Discussed in Thread: ADS1235-Q1 , LM53600-Q1 This is a not often seen request, but I have a customer asking me what the thickness of the thermal pad is for the VQFN version of the ADS124S08 (ADS124S08IRHBR)
Regards…