Part Number: LM53601-Q1 Customer is having issues with TPS536015 going into hiccup mode on 10% of their board assemblies and not recovering. The TPS536015 is used to generate a 5V supply that powers downstream regulators generating 3.3V, 2.5V and 1.2V…
Part Number: LM53601-Q1 Hi Team,
Does the treset_filter apply to VIN as well as the FB input?
For example, if my input voltage spikes low (say to 3.3V) very quickly and crosses the UVLO threshold (which can be as high as 3.55V), but the Vreset threshold…
Part Number: LM53601-Q1 Hi E2E,
I meet a question about LM536015. My product is a BOX, and LM536015 is assembled on the board. Then my BOX is working at 125 ℃, I find that the current is increased 0.1A than the normal 0.3A@5V. When the ambient temperature…
Part Number: LM53600-Q1 I would like to use the LM53601-Q1-ADJ to produce 3.0V from an input voltage of Vin = 12V +/-15% (10.2 < Vin < 13.8 V). The desired output voltage is slightly below the recommended operating conditions given in Section 7…
Part Number: LM53601-Q1 Hello,
I have a question regarding input capacitor selection for the LM53601-Q1.
In section 9.2.1 of the datasheet (SNAS660B), an input capacitor (CIN) with a value of 10uF is recommended. Accordingly, the application schematic…
Part Number: LM53601-Q1
Hi,
My customers are using TI's parts to design their 48V system. Now they need do some work about functional safety, so they want to get the relevant user guide which include failure rate, typical failure mode, and so on.…
Other Parts Discussed in Thread: LM53601-Q1 Hi,
We got a question from the customer about LM53601-Q1. Could you help us?
[Question] Is there EMI data for Nissan NDS compliance?
Best Regards, tateo
Part Number: LM53601-Q1 Hi,
We got a question from the customer about LM53601-Q1. Could you help us?
[Question] How much is the maximum Enable input current? They don't need quarantee. They will use it as reference.
Best Regards, tateo
Part Number: LM53601-Q1 Hi,
We got a question from the customer about LM53601-Q1. Could you help us?
[Question] How much is the maximum SYNC/MODE leakage current? They don't need quarantee. They will use it as reference.
Best Regards, tateo