Jared,
LM53602-Q1 model failure under the desired test conditions is not due to dropout. It is because the calculated minimun Toff exceeds the typical value given in the data sheet 125ns.
You may want to create a design with a higher delta between Vin…
Part Number: LM53602-Q1 The design is not created by WEBENCH when using condition is Vin:8V, Vout: 6.5V, Iout: 1.5A. What limits the design?
Don't we use LM53602-Q1 for this using condition?
Best Regards, Kohei Sasaki
Part Number: LM53602-Q1 Hello,
Could you provide me with the possible Min and Max input voltage threshold for mode change in AUTO Mode? Figure 13 on page 16 of LM53602-Q1's data sheet shows only a typical curve, but what I ask for is the Min and Max curves…
Part Number: LM43602-Q1 Other Parts Discussed in Thread: LM53602-Q1 , LM43602 , LM53603
Hello,
I'd like to ask some questions about LM43602-Q1.
At the input voltage of 6 to 6.5 V that will not rise further, will a LM43602-Q1 switch its switching mode…
Part Number: LM53603-Q1 Other Parts Discussed in Thread: LM53603 , LM53602 Hello,
I have question based on datasheet LM53603/602, there is a sync pin (input only) but are we capable to have a syncout too?
Meaning does the sync pin is dual function input…