Part Number: LM53635-Q1 Hi
Please let me ask you about LM53635.
If the Vout overshoot at transient response, can this device turn on the Low-side FET to suppress the Vout?
Best regards,
Yokota
Part Number: LM53635-Q1 I am using LM53635-Q1 model to compare the values reflected by WEB bench , TINA TI and then comparing it with actual values which i will get in the LAB with hardware chip. I have to do efficiency analysis and check the loop compensation…
Part Number: LM53635-Q1 Dear all,
one of my AA, is interested to know if the LM53635-Q1 can sustains the following pulse test:
ISO 7637 Test 1
ISO 7637 Test 2a
ISO 7637 Test 3a
ISO 7637 Test 3b
In case the part cannot sustain them. Can you…
Part Number: LM53635-Q1 Other Parts Discussed in Thread: TIDA-00987 Hi Team,
1. Can TPS53635 passed CISPR25 level 5 without spear spectrum function?
2. What is the side-effect of spear spectrum function? Eff? anything else?
Thank you.
Part Number: LM53635-Q1 Hi Sir,
in some TI chip, we have a Pin to Pin short test(typically two close pin) to make sure that out chip will not damage and will be back to normal if the short condition removed.
Do we have such report or test result on…
Part Number: LM53635-Q1 Hi all We are using the LM53635 SMPS for an automotive design. The device supports up to 36V input and tolerates 42V spikes. From previous experience, we think some additional input protection is needed to ensure that the device…
Part Number: LM53635-Q1 About Input Capacitor Selection is in LM53635-Q1 datasheet P25.
There is the description that "TI recommends that a small case size 10-nF ceramic capacitor be placed across the input, as close to the device as possible." Is this…
Part Number: LM53635-Q1 Hi,
I found the Vout max is 10V. I would like to know why it has this limit? Can I have any chance to design a 15V output?
Thanks.