Part Number: LM60430-Q1 Other Parts Discussed in Thread: TPS22968 , LM60430 Dear,
As stated in this FAQ I am opening a thread because I can not find the LM60430-Q1 model in PSpice for TI. I made sure I updated the libraries.
There seems to be a similar…
Part Number: LM60430-Q1 Hi Team
What is the problem with the following conditions?
Input 24V, output 12V/3A
Input voltage drops slowly to 9V
Whether the output voltage can be maintained above 8.6V
Part Number: LM60430-Q1 When the values of components given in the data sheet are put into the simulation program they do not even come close to passing CISPR 25, and when I use just the simulation tool, minor changes cause erratic changes in other components…
Part Number: LM60430-Q1 I have had one TI Power Designer design fail conducted emissions and attached is a second new design that uses the same parts as the evaluation board.
I need some assurance that this new design will pass conducted emissions testing…
Part Number: LM60430-Q1 Hello team,
Due to a stock problem, my customer is considering LM60430-Q1 for their project. Their project uses the Raspberry Pi zero (1GHz) as their edge compute. They will use the LM60430-Q1 as a 24 to 5 V DC-DC converter. They…
Part Number: LM60430-Q1 rant rant rant
I do want to use a TI part, but I am not impressed that a TI part that is advertised as meeting CISPR25 standards still needs an input filter. I also find it very troubling that the values given in the data sheet…
Part Number: LM60430-Q1 Other Parts Discussed in Thread: LM60430 , LMR33630 Hi Team,
It appears that Webench won't simulate the LM60430-Q1. Any idea why this isn't working? Do you have any other suggestions for alternative devices that we could use to…
Part Number: LM60430-Q1 I'm trying to figure out how large of an inductor value can be used with the LM60430-Q1 when the max load current is under 500 mA?
Using Webench, it recommends 10 uH, while the Quick Start calculator reports 60 uH. I'm worried…
Part Number: LM60430-Q1 Hello Guys,
Good day.
What is the power consumption rating for the LM60430AQRPKRQ1? It seems that this is not directly specified on the datasheet. Any estimated value/s?
Thanks!
Art