Part Number: LMQ66410 Other Parts Discussed in Thread: LM61480 , LM61495 , LM62460 , LMQ66420 , , LMQ66430
Hi support team,
Are the differences between LMQ66410, LMQ66420 and LMQ66430 the same as the differences between LM62460, LM61480 and LM61495?
・Current…
Part Number: TPS5450 Other Parts Discussed in Thread: LM61480 Is it possible to double the current capacity by bundling the two outputs of TPS5450?
Many LEDs have a common Anode, which requires a large current.
Please give me advice.
Part Number: TPS54561 Other Parts Discussed in Thread: LM61480 Referencing:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1226147/lm61480-q1--5v-inverting-output-possible
Current PCB uses TPS54561 for +5V…
Part Number: LMR43610-Q1 Other Parts Discussed in Thread: LM61480-Q1 Hello TI,
We are checking the input range of LMR43610-Q1, and wondering if there is a specification of VIN sustained to transient like LM61480-Q1 list in datasheet? Thank you.
LM61480…
Hi Sam,
Yes, LM62460, LM61480/95 have the similar thermal spec.
I drew the circuit in the picture below. Please compare the final voltage with the voltage of each channel, and then give it to FB pin. Thanks.
Aurora
Part Number: TPS51396A Other Parts Discussed in Thread: LM61480-Q1 , Hi,
I need Iout(max) 8A buck regulator with Vin(min)- 4.5v and Vin(max) 24v and Vout is (5V) for automotive purpose. I need alternate part for this specification. Can you suggest some…
Other Parts Discussed in Thread: LM61495 , TPSM63608 , TPSM63610 , LM61480 I need one 15V -> -5V Regulator, where load current will be around 2.8 to 5A. at 75C ambient Temperature.
Kindly, suggest me some regulators either with integrated Inductor or integrated…
Part Number: LM62460 Other Parts Discussed in Thread: LM61495 , , LM61480 , LM3489 , LM25148 Hi Team,
My customer is designing a 12~24Vin, 12Vout power, when 12Vin = 12Vout, they hope that the controller can close 100% duty(H side SW fully turn on) as possible…
Part Number: LM3150 Other Parts Discussed in Thread: LM61480 , LM5146
I used LM3150 to make a power converter with 10-26V input and 5V 8A output voltage. However, the output voltage is 5.6V under no-load or light load.
When the load is greater than…
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS565208 , TPS51397A , LM61480 Hello!
I'm working with WeBench and was wondering what losses were modeled in the simulation. Conduction losses? Switching losses? AC losses?
Also,…