Part Number: LM3150 Other Parts Discussed in Thread: LM61480 , LM5146
I used LM3150 to make a power converter with 10-26V input and 5V 8A output voltage. However, the output voltage is 5.6V under no-load or light load.
When the load is greater than…
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS565208 , TPS51397A , LM61480 Hello!
I'm working with WeBench and was wondering what losses were modeled in the simulation. Conduction losses? Switching losses? AC losses?
Also,…
Part Number: LM5145 Other Parts Discussed in Thread: CSD18563Q5A , LM61480 Design Requirements:
Input Voltage Range: 9V - 36V
Output Voltage: 5V
Output Current: 8A
Max Allowable Voltage Ripple (peak to peak) : 100mV
Find the attachment below that contain…
Hello,
Here are some examples:
LM53625/35-Q1 2.5/3.5A
LM63615/25-Q1 1.5/2.5A
LM61480-Q1 8A
LM62460-Q1 6A
LM61495-Q1 10A
The 2+1+1 phase configuration would need to defined in the NVM of the PMIC. This cannot be changed during runtime. Either you can choose…
Hi DP,
The converters that you've listed may not work since the negative current limit of the device may be as high as -3.2A for LM61480 (8A).
The LM73606 may work since the typical negative current limit is -6A but I would budget for slightly higher…
Hi Samuel,
and what about the LM61480-Q1 and LM62460-Q1 which are presented in the same datasheet, will they follow the same scheduled release date?
Thanks.
Part Number: LM61495-Q1 Hello,
I've been informed to contact you for my question regarding PLM61495QRPHRQ1, I can't find the footprint of the product regarding the pad dimensions and their relative positions. Can you provide this information? …