Part Number: LM61495-Q1 Hello Team,
My customer is using LM61495-Q1 for up to 10A current driving. (nominal 6~7A).
Could you please kindly review the schematic and let me know if you have any concern or advice?
Thank you in advance.
Part Number: LM61495 Tool/software: Hello team,
I have just one question.
in this graph, why Vout decreases as the Iout increases?
I think duty affected by Iout. So, duty is already max, and Io is increased. duty can't be increase more, finally…
Part Number: LM61495-Q1 Tool/software: Over at digikey...
https://www.digikey.com/en/products/detail/texas-instruments/LM61495QRPHRQ1/14004426
Click on the data sheet and the pinout is 16 pins. Scroll down to the mechanicals and its 22 pins. Their…
Part Number: LM61495 Tool/software: Hello,
www.ti.com/.../lm61495.pdf
I plan to use 16V input and 3.3V output (fix).
Is it ok to apply voltage to EN (pin 13) before 16V is applied to VIN1 (pin 14) and VIN2 (pin 2)?
Are there any voltage regulations…
Part Number: LM61495 Tool/software: Hi,
I'm trying to simulate the LM61495 in PSpice, and I'm getting weird efficiency measurements. WEBENCH and the datasheet both say that I should be getting around 96-97% efficiency, but when I measure in PSpice,…
Part Number: LM61495 Tool/software: Hi Team,
Do we have dual-output buck device? Input is from 15V-25V, output needs one +5V and one -5V, output 50mA for each channel. Thanks in advance.
BRs,
Francis
Part Number: LM61495
Tool/software:
Hi,
I am currently in the process of designing a buck converter using LM61495 to step down my 8s Li-ion pack voltage from 29.6V to 5.3V. The rated current is around 2A and the peak current is about 7A. I will…
Part Number: LM61495 Tool/software: Hi teams,
I was wondering if the IC comes with output discharge function since the data sheet said "In this scenario, such as a shorted input test, the output capacitors discharge through the internal parasitic diode…