Part Number: LM61495-Q1 Hope you are doing good.
We have designed 3.3V VR using LM61495-Q1.
Vin=12V,Vout=3.3V,Iout=5A.
Could you please share us the efficiency results for 600khz, 800khz and 1Mhz.
Attached image FYR of current design
Currently we have…
Part Number: LM61495-Q1 Team,
Can we guarantee a min max duty cycle @ 400KHz ? datasheet only provides a typ at 2.2MHz. customer has to be able to work at low vin.
thanks
Part Number: LM61495 Other Parts Discussed in Thread: LM73605
Hi team,
I can't find a excel tool for custom design only webench,
customer use 28Vin convert to 17.5V output, Iout TDC is 7.5A
how should they pick the "output cap" and "frequency" to…
Part Number: LM61495-Q1 Hi TI expert,
I would like to ask a genernal question for all power VR.
Just use LM61495-Q1 to do an example.
VIN 9~16V , VOUT 8.82V operation frequency 400Khz
when VIN=9V ,VOUT 8.82V(duty 98%), in this moment whether VR work normally…
Part Number: LM61495 Hi Team,
A buck converter output 10V/6A
B buck converter output 0.5V/6A
Supply uLED power, as follows
what's issue with this design?
Part Number: LM61495
Hello team,
What is the maximum and minimum RSPSP (kohms) for Output Ripple with Ripple Cancellation? I would like to know how much range of RSPSP (kohms) that LM61495 accepts. In the datasheet, the resistor is usually around 20 kΩ…
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495RPHEVM Hi Ti Experts, hope you are going well.
Do you have more detail design information for the Filter?
And what's the affect if i delete the 74279226101?
many thanks
Part Number: LM61495 Hello support team
My customer would like to add diode into LM61495, to prevent reverse current when input power source is removed. Do you see any issue for this usage?
Thanks,
Koji Ikeda
Part Number: LM61495 Hi Team,
I'm running the Pspice simulation with LM61495RPH device using external sync.
I have SYNC input connected to Clock source:
But I cannot see SW output voltage to be synchronized to SYNC input frequency:
Please, advice…
Part Number: LM61495 Other Parts Discussed in Thread: TINA-TI , PSPICE-FOR-TI The Pspice (LM61495_TRANS.LIB) model for this component appears to be encrypted, as signified by:
Line 76: $CDNENCSTART_ADV2
Line 688: $CDNENCFINISH_ADV2
Is there an unencrypted…