Part Number: LM62460
I want to build a switching regulator with a variable output voltage (through a variable resistor FBB). I simulated various output voltages in Webbench, initially without changing the proposed circuit.
At 14V the power loss in…
Part Number: LM62460 Other Parts Discussed in Thread: TPS2663 I am using an LM62460 in a design of mine and it keeps failing in tests. It has 28VDC going into it and typically draws under 1.5A when it seemingly randomly fails (failures have happened at…
Part Number: LM62460RPHEVM Other Parts Discussed in Thread: LM62460 Tool/software: Hi
I'm working with TIDA020047 board, but i need to power on my TIDA020047 with 24V instead of the recommanded input power 12V. so should I modify the refernce design…
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM338 Hello everyone,
i have to deliver 5A to a varying load (between 1 ohm to 6 ohm) for about 1.2 seconds. My supply voltage is about 30V. On my first test circuit i used the LM338 voltage regulator…
Part Number: LM62460-Q1 Hello upon downloading the excel calculation spreadsheet , there are comment boxes , which cannot be moved, I cannot access the cell to use the spreadsheet
Part Number: TIDA-020047 Other Parts Discussed in Thread: LM62460-Q1
Tool/software:
Hi
I was wondering if I can power my board tida 020047 with 24v in stead of 12v as it mentioned in ti document.
Regards
Hello Alex,
You can use this device if you would like to. We also have a single output device that is in preproduction. Please see link below.
LM70880-Q1 data sheet, product information and support | TI.com
This device is rated to 8A continuous output…
Part Number: LMQ66410 Other Parts Discussed in Thread: LM61480 , LM61495 , LM62460 , LMQ66420 , , LMQ66430
Hi support team,
Are the differences between LMQ66410, LMQ66420 and LMQ66430 the same as the differences between LM62460, LM61480 and LM61495?
・Current…
Hi,
If your application needs to be 2.2MHz, then it is suggested to use the 6A variant (LM62460) device. For 400kHz you can use either LM61480 for 8A or LM61495 for 10A.
Regards,
Jimmy
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM62460 , LM61495 Hello Team,
I would like to know what is the maximum output current for the LM61495-Q1 at 2.2MHz operating frequency. Datasheet figures are showing different results. In the first…