Part Number: LM70840-Q1 Other Parts Discussed in Thread: LM62460-Q1 , LM61495-Q1 , LM61480-Q1 , LM62460 , LM70880-Q1 Tool/software: Hi, Team
I got three questions from customer regarding LM70840-Q1 functional Safety.
1. is this device satisfied with ISO26262…
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 Dear teams,
My customer is using LM62460-Q1. I have checked the DS and function safety document, while it seems that this device does not have internal function safety diagnostic feature…
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 Hi
im trying the attached circuit on my PCB: On my first PCB the circuit does not work as expected, i receive 2.8V rather than 5V and the reset pin is low indicating that the IC is fault…
Part Number: LM62460-Q1 Hello Team,
Are ICs able to work as an inverting buck-boost converter?
- LM61495QRPHRQ1
- LM61480QRPHRQ1
- LM62460QRPHRQ1
Thanks.
Regards,
Hirata
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 Dear TI,
I am working on the thermal design of LM62460 based converter and I have some questions regarding the IC thermal properties.
RthJB is given in datasheet and a note in layout chapter…
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 , LM73606 Hi team,
My customer considers to use LM62460 as alternative option of LM73606 because of delivery issue.
Could you please pin pitch which is marked as red circle in below screenshot…
Part Number: TIDA-020047 Other Parts Discussed in Thread: LM62460-Q1
Tool/software:
Hi
I was wondering if I can power my board tida 020047 with 24v in stead of 12v as it mentioned in ti document.
Regards
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460
Hello
I need help with determining of phase margin. We need to use this buck converter at specific operation conditions: Vin=5.2,9,15,20 and Vout=5V/3A. Based on the PSPICE simulation, the…
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 , LM62460 , LM61480 Hi I see in the datasheet that for the three part numbers: LM61495, LM61480, LM62460 they are rated for 6A,8A, and 10A, and are drop-in pin-compatible. However, I don't see…
Part Number: LM62460-Q1 Hello upon downloading the excel calculation spreadsheet , there are comment boxes , which cannot be moved, I cannot access the cell to use the spreadsheet