Hi user5351218,
Sorry for the delayed response. I am not very familiar with this device. Below is my interpretation of the datasheet.
My understanding is that yes, the PID's output directly becomes the PWM's signal.
When the motor speed increases…
Part Number: LM629 I have this question from my customer: I just have a quick request. I’m using the LM629 motor controller chip and wondered if TI has some sample code in
C that I can modify for my application. It’s a one-time project & I’m using…
Part Number: LM629 Hi
My customer is using the LM629 and would like to know what the difference is between the
LM629M-6/NOPB and the LM629M-8/NOPB.
Both are SMD, both are 24 pins, package quantity is the same.
The list at the end of the datasheet shows…
Part Number: LM629 Resolution of rotary encoder = 63E6 AqB counts/revolution. This is resolution coming out of 1000x interpolation circuit.
I'm using LM629M with 8 MHz clocking.
Other Parts Discussed in Thread: LM629 HI
we have some problem to detect missing signal encoder by using LM629N6 ,
does you have any solution to detect missing signal encoder in order to avoid to have pwm at 100% when encoder is disconnected ?
this problem…
Part Number: LM629 I see LM629's datasheet said the LM629 provides 8-bit, sign and magnitude PWM output signals for directly driving switch-mode motor-drive amplifiers.This means there are only 128 kinds of duty cycles.
I use speed mode and PID filter…
Part Number: LM629 Hi
Question1: does the LM629N6 dip version becomes obsolete ??
Question2: does it exist other ic like LM629n6 ?
Question3: does the LMD18200t becomes obsolete ??
best regards
Part Number: LM629 Hi
can i give 3.3V as input and control signals to LM629
AND for the 3.3V input,Is it produce output signals(HI,PWM SIGN and PWM Magnitude) in 3.3V range.
Part Number: LM629 Hello! everyone
I am a beginner with this platform and I have a question about How I can program the LM629. Do I need a pic programmer to download my algorithm? I would like download the code from Matlab with TCP/IP.
appreciate you…
Part Number: LM629 Hi Team,
My customer is using the LM629N-6/NOPB and since it is now in lifetime buy status, they'd like to know the suitable alternative.
I see online that we recommend the LM629M-6/NOPB as the alternative.
All I can see from the…