Part Number: LM63615-Q1 Hi team,
LM63615-Q1 has two threshold as Vreset_HIGH and Vreset_LOW. I guess these are rising threshold and fallinf threshold. Is it correct? For example, the device set 5V fixed, when output voltage rises 5.6V for RESET_HIGH…
Part Number: LM63615-Q1 Hi TI Team,
I am working on heatsink design for Buck converters and would like to confirm the correct method/formula for calculating the IC power dissipation (PD).
Should the IC power dissipation be calculated using:
PD …
Part Number: LM63615-Q1 Other Parts Discussed in Thread: LM63635-Q1 , Hi team,
Customer is concerned about lin regulation of LM63615-Q1 and LM63635-Q1.
I see Figure 8-16 to 8-19 for similar data, and Figure 8-34 to 8-37 for Dropout Voltage versus…
Part Number: LM63615-Q1 Hi Team,
We are developing LM63615DQDRRRQ1 as 12V-5V buck converter. While during the test, there is a large vibration, the SW frequency takes long time to be stable.
I guess the reason might be the loop is not stable. So…
Part Number: LM63615-Q1 Tool/software: Hello,
I'd like to receive the LM636x5-Q1 3.5V to 36V, 1.5A and 2.5A, Automotive, Step-Down Voltage Converter unencrypted Spice Model compatible with Nexxim Solver (Ansys Circuit).
Would that be possible from…
Part Number: LM63615-Q1 Tool/software: Hi Team,
Could you help to explain more about below describe in datasheet?
"Valley current limit prevents inductor current run-away during short circuits on the output, while both peak and valley limits work…
Part Number: LM63615-Q1 Other Parts Discussed in Thread: LMR33640 , LMR33610 Tool/software: Hi TI Team,
I have designed an IBB circuit using the LM63615-Q1 IC, referencing the application note. The design schematic is attached for your review.
Could…
Part Number: LM63615-Q1 Tool/software: Hi Team,
Harman uses the following chips in the platform, please help provide components detailed model:
3V3 buck-LM63615
4026465
Here is the requirement for detailed model:
Ecxml…
Part Number: LM63615-Q1 Tool/software:
I am measuring SW node voltage of LM63615DQPWPRQ1, I could witness the sudden dip in rising edge of sw node and it is rising again. can you please explain why this behavior and how to mitigate this
Part Number: LM63615-Q1 Other Parts Discussed in Thread: TSD24-Q1
Tool/software:
Hi team I'm planning to use the LM63615DQPWPRQ1 in a 24V system. Please recommend a suitable TVS for IC protection