Part Number: LM63625-Q1 Other Parts Discussed in Thread: LM63615-Q1 , Tool/software: Hi team,
The LM63625-Q1,LM63615-Q1 data sheet doesn't list Efficiency curve at FPWM mode.
Is it possible to get a curve of power supply efficiency…
Part Number: LM63625-Q1 Tool/software: Hi team,
My customer requests followings, could you support?
Customer use case : Vin = 14V, Vout =5V, Iout = 300mA, Fsw=2.1MHz, FPWM( or Auto mode)
(1) Could you provide below data when Iout = 0A to 300mA…
Part Number: LM63625-Q1 Hi there,
I ran into some problems when I tried to use LM63625 Q1-Transient PSPICE model embedded in PspiceforTI to run ac sweep. (Vin=12V, Vout=3.3V, Iout=2A)
The bias point it calculate it's not in steady state, so the ac…
Part Number: LM63625-Q1 Hello Expert,
We'd like to confirm EN pin status when Vin is removed? Could you please provide this information?
I suspect that it is Hi-z but I'd like to make sure about it.
Best regards, Kazuki Kuramochi
Part Number: LM63625-Q1 Hi team,
The customer are using TPS63625 buck regulator as always on power for 3.3V power supply.
It can be understood that as a long-term power supply, when other parts of the host are not working, this power rail provides…
Part Number: LM63625-Q1 Hi Team,
We are using LM63625DQPWPRQ1 in SMPS section to convert 12V to 6.8V in our application. While Vin is falling, it is observed frequently that the IC output top switch is getting failed.
Kindly share some light into…
Part Number: LM63625-Q1 Hi,
I have implemented a 24V to 3.3V configuration and during testing two LM63625 have faulted in the same way, they internally short (0.9 ~ 1.1 ohm) the output to ground resulting in high current draw and heating of the device…