Part Number: LM64460-Q1 Hi,
Can you please the review the following circuit for LM64460A, with input as 9V and output as 3.3V at 3A at a switching frequency of 2.1M?
I have generated this circuit from WEBENCH designer and followed the evaluation board…
Part Number: LM64460-Q1
I'm using the design provided by Webench
The forum seems to be filtering the Webench design link below. The design parameters are Vin: 8V to 16V with 13.2V nominal. Vout = 5V fixed, Iout: 0 to 0.7A, 0.1A nominal
link: Webench…
Part Number: LM64460-Q1
Hi support team,
What are the specifications of LM64460APPSRYFRQ1?
https://www.ti.com/product/LM64460-Q1/part-details/LM64460APPSRYFRQ1
There is no description in SNVSBW0.
Regards,
Dice-K
Hi, thanks for the response!
Yes, I did go through the steps to enable macros and ActiveX on the 'Instructions' sheet. Although configuration menus changed a bit on the newer versions of Excel, they remain valid.
And I know macros are enabl…
Part Number: TPS62442-Q1 Other Parts Discussed in Thread: LM64460-Q1 Hi,
I am designing a DC-DC buck regulator with 3.3V input and 2.5V and 1.2V as outputs, I have used TPS62442-Q1 and followed the WEBENCH design for this. I also need this circuit to…
Hi Minoru,
LM63460-Q1, LM64460-Q1, and LM76005-Q1 both have FPWM option.
Note the LM63460-Q1 will require specific IC number.
Hope this helps,
-Orlando