Part Number: LM65645 Other Parts Discussed in Thread: LM5148 Hi experts,
Good day.
My customer has a 100W BUCK new demand. EE: Knitting machine.
Is this socket suitable for using in this scenario? WEBENCH shows below power loss. Or do you recommend…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 Dear TI team,
I would like to use LM65645 used as the primary buck to 5V output.
The background shown as below:
Input Voltage range: 6V~36V
Output Voltage: 5V
Output current: …
Part Number: LM65645 This is a continuation of topic
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1664697/lm65645-dc-dc-doesn-t-start-normally-when-load-is-connected/
Because that conversation has already…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 LM_65465_Schematic print.pdf
Dears,
i open this thread because i have questions about Lm65645 usage. I have a 45V<Vin<55V (Vout_BOOST in the pdf file) and 4 different LM65645 to produce…
Part Number: LM65645 Hi,
We are using LM65645 in our design for generating 5V @3A. In LM65645EVM Evaluation Module , we could see that there is a 100uf 63V ALUM capacitor. due to height issue we are not able to include this part in our design, since…
Hello,
We've used LM65645RZTR in our PCB design to step down the 4S-6S liion battery voltage down to two 5V power domains (i.e. 2 parts per board). As the boards arrived, I inspected a few and the output seems very off. Out of 3 boards, 4 regulators…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 I need a power output that can easily vary between 5V and 5.5V.
I am considering bridging the feedback pin of LM65645 from a calculated 5.5V output with 2-resistor, to short circuit…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 Hello T.I. teams end users,
I hope everybody are doing well.
I am currently using a LM65645 power converter IC to step 36VDC down to my 3.3VDC logic supply on a PCB.
Reading the datasheet…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 We are working on a design for a control board for an industrial robot. We are designing a 12 V buck regulator with an input voltage range of 33 V to 62 V; however, we expect large input…
Part Number: LM65645 Other Parts Discussed in Thread: , TPSM65630
Hi Team,
Posting on behalf of our customer.
I will share this post with our customer so he can reply when needed.
We created a prototype board based on LM65645. And encountered…