Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 Dear TI team,
I would like to use LM65645 used as the primary buck to 5V output.
The background shown as below:
Input Voltage range: 6V~36V
Output Voltage: 5V
Output current: …
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 I need a power output that can easily vary between 5V and 5.5V.
I am considering bridging the feedback pin of LM65645 from a calculated 5.5V output with 2-resistor, to short circuit…
Hi Angelo,
Angelo Ruotolo said: for all the listed configurations the best solution is to connect BIAS to externel 3.3V, efficiency-wise?
Yes. The bias pin supplies to the internal LDO whose voltage is ~3.3V. So regardless of the output conditions…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 Hello T.I. teams end users,
I hope everybody are doing well.
I am currently using a LM65645 power converter IC to step 36VDC down to my 3.3VDC logic supply on a PCB.
Reading the datasheet…
Part Number: LM65645-Q1 Tool/software: Hi team, Good day.
The Ultralibirian file uploaded for LM65645-Q1 doesn't have 3d-model. Help me found it, please. https://vendor.ultralibrarian.com/TI/embedded/?gpn=LM65645-Q1&package=RZT&pin=20&sid=0195191d3ae5001ec2dce45be3a10506f00a406701328&c…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 We are working on a design for a control board for an industrial robot. We are designing a 12 V buck regulator with an input voltage range of 33 V to 62 V; however, we expect large input…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65635-Q1 , Tool/software: Hello, Team,
We want to know whether we can P2P replace LM65645-Q1 and LM65635-Q1 without any concerns and change in the design.
Best, Masaru
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM70660 , LM76005 , LM68645-Q1
Tool/software:
Hi support team,
I am looking for an inverting buck-boost (IBB) converter that can achieve the following specifications.
VIN: 19~30.8V VOUT…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65645 Tool/software: In TI's workbench if you design a LM65645 supply using 12V - 48V in and an output current of 3A, the 3.3V, 5V or 12V as the output voltage, all use a 10uF inductor. This is…
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM68645-Q1 , LM68645 Tool/software: Hello Team,
Could you kindly send a " Functional Safety FIT Rate, FMD and Pin FMA " document of LM65645SRZTRQ1?
If there are no document, please provide safety…