Part Number: LM66100 Other Parts Discussed in Thread: LM66200 Hi,
I'm trying to use two LM66100 or a LM66200 for Oring a 5vdc power supply and a non rechargeable 3.6V Li-SOCl2 battery(only used when 5Vdc isn't available).
I also need to have a…
Part Number: LM66100 Other Parts Discussed in Thread: TPS2116
Hi,
I intend to use the LM66100+PMOSFET as the following design from datasheet
I have some questions which answers I can't find within EVM board or datasheet:
1. I want to double che…
Part Number: LM66100-Q1 I have used the above part to OR two power sources. Pin CE-bar of the 1st part is permanently connected to ground. Pin CE-bar of the 2nd part is controlled. There is a reverse current going through the 1st part when Vout is present…
Part Number: LM66100 I am considering the LM66100 configuration which would provide reverse current blocking from the datasheet:
The device turns ON when VCE is approximately 250mV BELOW Vin (VIN - VCE > 250mV)
Doesn't this mean that when using…
Part Number: LM66100 1.Have R&D engineers help to see why this circuit structure has a 6mA pour current (The electrical circuit diagrams are attached)?
2.There is a question about this circuit: If it happens that two LM66100 VIN's are equal in size…
Part Number: LM66100 Other Parts Discussed in Thread: TPS2116 Hi team,
Can I know what's our solution compared to ADI LTC4412?
LM66100-Q1 seems to be similar, but it can only achieve automatic switch between to power supply based on the voltage comparison…
Hi Patrick
LM66100 Maximum continuous current (IMAX): 1.5 A Current is too small At least 5A
LM74700D-Q1 or LM74502H. The minimum input is 4V, and the customer's minimum battery string is 3V. And these two controllers need to be used with external…
Part Number: LM66100 Hello,
I am posting this topic regarding the use of the LM66100 component. I am working on an externally powered device. I want to measure the voltage under charge of the battery.
The goal is to activate transistor Q7 for a very…
Part Number: LM66100-Q1 Other Parts Discussed in Thread: LM66100 , , LM66200 , TPS2116
Hello,
I am posting this topic regarding the use of the LM66100 component.
In my design, I have two 5V voltage sources(Vin1,Vin2), powering the output connected devices…
Hi Tyler,
Sorry for the delay on this. Can you also try connecting each VIN to the opposite CE pin? This may solve your issue. If this doesn't work, then we can discuss some more complex alternatives for this.
Thanks,
Patrick