Part Number: LM66100 Other Parts Discussed in Thread: TPS62933 I am building a circuit that I want 5V from POE and 5V from USB to power a device. The 5V from POE should take precedence but the USB should be able to be plugged in as well without either…
Part Number: LM66100 I read in the datasheet that the CE pin must not be left floating.
Now, please see datasheet "Figure 15. Dual Ideal Diode ORing"
Our application has one battery as power source and the other as a DC-plug for external power…
Part Number: LM66100 Hello,
We need to use the super capacitor charge from 3.3V with eFuse IC. Current would be around 200mA.
Will LM66100 block the backward current flow when 3.3V supply is zero or do we need to go for ORing the IC?
Let me know if any…
Part Number: LM66100 Dear Team,
If LM66100 is not connected the power supply to VIN(VIN is open),
When 5V is connected to VOUT, current consumpition is not sink to VOUT by body diode?
(Is LM66100 funcioned as Diode eve if VIN =0V?)
Best regards
Part Number: LM66100 In my application I need to switch between two power inputs but in some cases the VIN will be left unconnected and only the secondary input will be connected at CE.
According to the DS the input voltage range of the VIN pin is 1.5…
Part Number: LM66100 Dear Team,
Just to make sure,
About Typical Appilication's CL and RL,
Even If CL and RL is open, LM66100 is able to operation as no problem?
Best regards,
Part Number: LM66100 Other Parts Discussed in Thread: TPS2116 Hi,
I am planning to use LM66100 ideal diode for a battery powered application where I need to use two batteries in ORing configuration.
Before implementing the circuit in the actual product…
Part Number: LM66100 Hi everybody,
I want to charge 2 batteries in parallel with one charger.
When I use the battery in wrong polarity, I have a negative voltage at input of the LM66100.
How can I fix it?
Regards
Esmaeel Heidari
Part Number: LM66100 Hi !
I am using the LM66100 in one of my design to enable or disable a 5V net.
Vin is 5V. ~CE is receiving a signal coming from a 12V rail and divided by a resistive bridge to bring it down to 5.5V
The "12V" signal is enabled depending…
Part Number: LM66100-Q1 Other Parts Discussed in Thread: LM66100 , TPS2116 Hello Sir:
We want to use LM66100-Q1 on battery pack protection.
Our function requirements shows below.
1. only discharging from battery side to load side.
2. cannot charge battery…