Part Number: LM66100-Q1 Other Parts Discussed in Thread: LM66100 Dear Friend
I would like to use LM66100-Q1 in the same way as a P ch MOSFET for a high side load switch application.
From datasheet, it can be turned on with VCE <= Vin - 80mV and turned…
Part Number: LM66100-Q1 I have used the above part to OR two power sources. Pin CE-bar of the 1st part is permanently connected to ground. Pin CE-bar of the 2nd part is controlled. There is a reverse current going through the 1st part when Vout is present…
Part Number: LM66100-Q1 Other Parts Discussed in Thread: TPS63900 , LM66100 , TPS2117 Tool/software: Good evening,
I am designing a power supply system for an IOT sensors working with LORAwan,;
3 x Primary Cell (LiSoCl2 , 3.6VDC MAX, D Size ) in…
Part Number: LM66100-Q1 Other Parts Discussed in Thread: LM66100 , , LM66200 , TPS2116
Hello,
I am posting this topic regarding the use of the LM66100 component.
In my design, I have two 5V voltage sources(Vin1,Vin2), powering the output connected…
Part Number: LM66100-Q1 Other Parts Discussed in Thread: LM66100 , TPS2116 Hello Sir:
We want to use LM66100-Q1 on battery pack protection.
Our function requirements shows below.
1. only discharging from battery side to load side.
2. cannot charge…
Part Number: LM66100 Other Parts Discussed in Thread: TPS2116 Hi team,
Can I know what's our solution compared to ADI LTC4412?
LM66100-Q1 seems to be similar, but it can only achieve automatic switch between to power supply based on the voltage comparison…
Hi Rahul,
Welcome to E2E!
I am sorry to hear you are experiencing this at the late stages of HW design.
Our TPS2124 is not automotive qualified and not recommended for automotive operation. We do not have any automotive grade power muxes currently…
Part Number: LM66100 Other Parts Discussed in Thread: LM7310 Hello TI Support Team,
We are designing a power OR-ing circuit using three LM66100DCKR devices for a battery backup application and would like your review on the overall approach and a specific…
Part Number: LM66100 Other Parts Discussed in Thread: LM74502H , LM74700D-Q1
Hi
Please advise on products that can replace the LTC4450
p2p is better, Tks