Other Parts Discussed in Thread: LM66200 , TPS2121
I am using the LM66200 to controle the power Supply for a 5V Regulator. Maximum of 10W to 12W on the 5V_MAIN is needed.
In this case, the 5V voltage must not drop.
VIN1 and VIN2 of the LM66200 is…
Part Number: LM66200 Other Parts Discussed in Thread: TPS2116 , TPS2117
Hi,
I am using LM66200DRLR in one of our products for input voltage selection and reverse current protection between two battery packs. Please refer to the image.
So far, out…
Part Number: LM66200 Other Parts Discussed in Thread: TPS2116 I have 2 input power source, and I am using LM66200 IC for ORing the suppies. The regulated 5V from the battery and the 5V from USB. Please find the circuit diagram attached. To make sure the…
Part Number: LM66200 Tool/software: Our product requires flexible power supply using multiple non-rechargeable batteries, with application scenarios involving 2, 4, or 6 batteries. The batteries we use are non-rechargeable lithium-manganese batteries…
Part Number: LM66200 Hi-
Customer is looking at using LM66200 for simple reverse current blocking. Vout is 5V and need current output of >=2.5A. Can you help with question below?
It wasn’t clear from the datasheet what to do with the unused input…
Part Number: LM66200 Hi team, Does reverse current protection only become active when Vin < Vout and a current of 1.4A (TYP) flows? The other words, does reverse current protection not function with only the condition VIN < VOUT? BR, Kengo.
Part Number: LM66200 The Datasheet ( www.ti.com/.../SLVSG04) of LM66200 describes the pin ST (status) in Table 5-1. Pin Functions as
" Status pin. Pulled high when VIN1 is being used and pulled low when VIN2 is being used. Can be pulled up to VIN1 to…
Part Number: LM66200 Hi All, Title:Vout when switching from VIN1 to VIN2 I have a question about the LM66200DRLR. When the input voltage switches from VIN1 to VIN2, VOUT is not output for approximately 3ms. The LM66200DRLR datasheet states that the tSW…
Part Number: LM66200 Tool/software: Hello,
I would like to ask you a question about the soft start of the LM66200. The VOUT rise waveform was measured with VIN1 set to 3.3V and VIN2 set to 0V. The VOUT rise time was 19us, which is quite short. Are there…