Part Number: LM66100 Other Parts Discussed in Thread: LM66200 Tool/software: Dear TI team,
We would like to get your recommendation regarding ORing two power sources on our PCB.
Our current design involves powering the device with a single-cell…
Part Number: LM66200 Tool/software: Dear TI Engineer,
When we add input voltage on both VIN1 and VIN2 of LM66200, the output voltage is only 0.5V. But when removing any of the VIN, the output voltage is normal. Also, if there is no load at the output…
Part Number: LM66200 Other Parts Discussed in Thread: TPS2117 Tool/software: Hi,
Is it ok to use 2 chips in parallel to double the current handling capacity like below circuit?
Thanks,
Part Number: LM66200 Tool/software: Hi,
We use LM66200 as power switch, Vin1 is primary supply (5V), Vin2 is supplied by a 2Fala capacitor, ON pin is connected to GND.
the load current is 600mA.. Normally the output is suppled by Vin1, it can switch…
Part Number: LM66200 Other Parts Discussed in Thread: LMR51430 , TPS2116 , TPS2117 Tool/software: Hello
I have a design where I am using the LM66200 to control whether the System Voltage is 5V from an USB Connector or 5V (output of LMR51430X). It…
Part Number: LM66200 Tool/software: Hello,
I am an FAE at a distributor that handles TI products. I received the following questions from my customer.
Please tell me about the function that automatically switches between VIN1 and VIN2. (Question 1…
Part Number: LM66200 Other Parts Discussed in Thread: TPS2117 Tool/software: Hi team.
Do we have higher current oring device? Current need is >6A, but I found that LM66200 only supports 2.5A. Input channel should be 2.
Nison
Part Number: LM66200 hi,
We encounter issue on using TI’s LM66200 power path controller in our product when we applying for IEC61010.
Will you be able to provide some advice on regards to the issue?
Best regards,
Felix
Part Number: LM66200 Other Parts Discussed in Thread: TPS2117 We are designing a system using the LM66200 where a DC power supply is connected to VIN1 and a primary Lithium battery is connected to VIN2. When the DC supply is higher than the battery voltage…