kai klaas69 said: You can understand the effect of snubber (Baucherot-, Zobel-network) only if you keep in mind that the output stage of OPAmp ( LM675 ) has a finite open loop output impedance, Ro. At unity gain frequency Ro and R of snubber must form…
Part Number: LM675 Other Parts Discussed in Thread: OPA549 Would there be a recommended torque requirement for a mounting screw that attaches to the thermal tab of the LM675 (TO-220 package)?
Part Number: OPA548 Other Parts Discussed in Thread: LM675 , Hi,
I need a power operational amplifier with following requiremeents: Vsupply=+/-12V; Ioutmax=0.8A. I found LM675 but in the datasheet it is said that it could have some stability problems…
Part Number: LM675
Hi team,
May I know why there are not NEB package and temperature shown in LM675T/LF02 datasheet ?
Customer plan to use LM675T/LF02 but they are Curious why it can't be found in datasheet ?
Do you have any suggestions?
Thanks…
Part Number: LM675 Hi
Our customer is evaluating LM675 and they have question.
There is possibility of being applied the voltage (+/-0.7V, 1.4Vpp) at the output (4pin) of LM675 while not powering.
Is this applying voltage to the output terminal…
Part Number: LM675 Team,
given a max height constraint of 15 mm, can the LM675 be mounted horizontally on the PCB? Do you see any issues?
Please let me know
It's an urgent matter.
Thanks
Hi Dominic,
The dies are slightly different, but they are essentially the same core device. The LM1875 was originally designed as an audio power amplifier, then was "spun" as a "power op-amp" as the LM675.
The main difference is how the two are tested…