Part Number: LM70660 Hi Teams,
Could you please confirm whether there is a minimum Rshunt limitation for LM70660?
We are currently using an Rshunt of approximately 4.78 mohm, with an OCP calculation of about 11.2 A. Would there be any potential issues…
Part Number: LM70660 Other Parts Discussed in Thread: LM5137 Hi,
Does LM70660 can support to 100% duty cycle?
Or other WV buck converter can support 100% duty cycle?
VIN= 30V
Vout=5V
output current >1A
Thanks!
Jeff
Part Number: LM70660 Hello Team,
I would like to confirm the connection method for the BIAS pin.
The datasheet states that the BIAS pin should be connected to GND when it is not used. However, if the pin is mistakenly left open, could this cause any…
Part Number: LM70660 Tool/software: Hi Team,
Customer use LM70660 with below layout questions, could you please help check them? Thanks.
Currently, they connected AGND with PGND, is it correct?
17-pin AGND and 30-pin PGND are connected together…
Part Number: LM70660 Other Parts Discussed in Thread: LM706A0 Hi team,
I have two questions regarding the LM70660, LM706A0, and LM708x0 devices:
When these devices are used at the same output current, are they pin-to-pin compatible, including…
Part Number: LM70660 Tool/software: I want to use LM70660 synchronous buck in my design, however I am not able to simulate the model in LTSpice as the library file is encrypted. Can you please guide me how to simulate and validate the working of LM70660…
Part Number: LM70660 Tool/software: Hi Team,
Could you please help to provide the efficiency data from 48V to 24V with 6A output current.
Thank you,
Yishan Chen
Part Number: LM70660 Tool/software: In section 7.4.2 in the LM70660 only shows the top layer of the layout example and I wanted to ask two things
1) Are there any intentions of adding another figure that shows the bottom side of that layout example…