Part Number: LM706A0-Q1 Hi,
I am planning to use the LM706A0-Q1 in one of my designs. My requirement is 12V/10A and 28V/10A. I have designed these circuits using WEBENCH. Please confirm whether these designs are feasible.
I would also like to know…
Part Number: LM706A0-Q1 Hello,
We have come up with 2 buck converter design using LM706A0-Q1. Both are 8.4V, one is 8A and other is 5A
8.4V 8A
8.4V 5A
Hopefully the screenshot has all the details.
I am also attaching the quickstart excel…
Part Number: LM706A0-Q1 Other Parts Discussed in Thread: LM70880-Q1 Tool/software: what is the maximum continuous current for 12V output out of a LM706A0-Q1?
Part Number: LM706A0-Q1 Other Parts Discussed in Thread: LM706A0 Tool/software: Hi all,
I use LM706A0 EVM board to test 48Vin/3.3Vout@max 10A condition and see the transient regulation out of 5%.
Transient condition is 4A to 10A with 2.5A/us, using…
Part Number: LM706A0-Q1 Tool/software: Hello Ti Forum,
I would like to know if you can use the LM706A0-Q1RRX IC, buck, for an inverting configuration?
Please refer any application notes for this IC that are relative to the IBB or just Inverting configuration…
Part Number: LM706A0-Q1 Tool/software: Please provide efficiency graph, Derating Graph, Recommended Switching Frequency, Short Circuit Recovery for an input range of 13 to 60V and output of 120W (max) at 12V and nominal of 108W at nominal. Also please…
Part Number: LM706A0-Q1 Other Parts Discussed in Thread: LM706A0 , LMQ61460 , LM70880-Q1 Tool/software: Hello Ti forum,
I would like to know what the reference plane is for the Switch Node when using the LM706A0 -Q1 in IBB configuration.
1. Is the…
Part Number: LM70880-Q1 Other Parts Discussed in Thread: LM706A0-Q1 Tool/software: I created a 12V, 24V OUTPUT Module using LM70880-Q1.
The input voltage range is 40V to 60V, using a 48V battery.
The circuit diagram used for the module with 12V and…
Hi Carlos,
Carlos Sarille said: Is it correct to assume that the values for the compensation network calculated for 1-device operation are valid also for parallel configuration?
Yes, that is correct.
Carlos Sarille said: The question is, for light…
Hello, sorry for the issue. The device can support 24V, but it is my understanding that for a 24V battery load dump profile, the voltage may exceed the absmax of hte device.
In that case, you may want to consider a higher intput voltage device to support…