The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: LM70840-Q1 Other Parts Discussed in Thread: LM70880QEVM Tool/software: I need the Gerber files for the EVM LM70880QEVM to compare the thermal pad requirements.
Part Number: LM70840-Q1 Tool/software: Hello! On Page 15 of the data sheet, the following is shown : "The configuration settings are latched and cannot be changed until the input voltage to the LM708x0-Q1 is recycled." Does this mean if I connect…
Part Number: LM70840-Q1 Tool/software: Could you please provide the symbol and footprint files for Part Number LM70840-Q1 in .edx or .hkp format, as required for the Xpedition Mentor Graphics tool
Part Number: LM70840-Q1 Other Parts Discussed in Thread: LM70840 , LM70880 Tool/software: I need to design a buck converter with below specifications:
Input voltage: 17V to 63V.
Output voltage: 12V.
Load current: 1.5A max.1.2A Typical.
Ambient temperature…
Part Number: LM70840-Q1 Tool/software: Hello,
We are implementing LM70840QRRXRQ1 in one of our designs.
Vout is set to 5V so FB is connected to VDDA through a 24,9K resistor.
How the loop stability measurement could be performed in this case?, where the…
Part Number: LM70840-Q1
Tool/software:
Dear Sir or Madam,
we have implented follow regulator in our design: LM70840QRRXRQ1
The regulator does what it is supposed to do.
But the reaction of different speeds of driving up the input voltage is very different…
Part Number: LM70840 Other Parts Discussed in Thread: LM70880 , , LM70860 Tool/software: Hello, could you please elaborate on the differences of LM708x0 variants (LM70840 vs. LM70860 vs. LM70880). We could use the LM70840 for our application, but using the…
Hi Nagata-san,
Is there any feedback? If not, go ahead and close the thread. You can open another thread once you hear back from the customer. Thanks!
Ben