Part Number: LM70860-Q1 Other Parts Discussed in Thread: LM70860 Hi Teams,
The customer is using LM70860 to develop the power board for the robot. Please help review the schematic diagram to see if it is reasonable.thank you~
Part Number: LM70860-Q1 Other Parts Discussed in Thread: LM70860 Hi TI Team,
I am designing a synchronous buck converter using the LM70860-Q1 . My design target is to support a continuous load of up to 6A . However, the system triggers OCP (Over Current…
Part Number: LM70860 Let me ask one simple question. I got a WEBENCH report for LM70860RRXR like below. Dose that mean rated voltage 50V is enough? the value should be 4.8926nF at 26.4V vias?
Part Number: LM70860 Hi ,
I would like to know if it is feasible to use LM708x0 to generate a negative voltage from a positive voltage?
My basic idea is to create an AC/DC module including a PFC, 2x DCDC 400V to 40V (one for digital and one for analog…
Part Number: LM70880 Tool/software: There are some discrepancies between schematic in datasheet, PDF dev board one, and Altium dev board schematic.
In particular Altium dev board schematic has extra components not present in other schematics or Webench…
Part Number: LM70860 Other Parts Discussed in Thread: TPS54560 , LMR16030 , , LM5137 , LM25085 , LM25137
Hello TI,
I am looking for a buck with 100% duty cycle or something like "pass through switch feature" when Vin=Vout. Buck converter will power…
Part Number: LM70860-Q1 Other Parts Discussed in Thread: LM70880-Q1 , LM70860 Tool/software: Hello,
If you have the Altium footprint file for the part number LM70860-Q1, can you share it?
Can you share the design files of the Eval boards for the part…
Part Number: LM70860-Q1 Tool/software: Hello,
I will use the LM70860-Q1" integrated circuit in an automotive ECU, I could not find any information about reverse polarity protection in the datasheet, I would be glad if you could answer the following…
Part Number: LM70860-Q1
Dear TI experts,
my customer made their PCB using LM70860-Q1.
During the test they found that current consumption of product in sleep mode is little high.
Could you review the schematic first?
(Please refer the design…