Part Number: LM70880-Q1
Tool/software:
Hello ,
I have downloaded the PSPICE simulation file from the TI website.
I am not able to simulate the project file, it is showing some error when i run it without modifying anything from the schematic.
I have…
Part Number: LM70880-Q1 Other Parts Discussed in Thread: LM70880 , LM70860 Tool/software: Hello,
My customer requested TI's review of the LM70880-Q1 design.
Please review their design below to see if there are any problems.
LM70880-Q1 REF SCH_20240911…
Part Number: LM70880-Q1 Tool/software: Hello,
My customer is looking for a DC/DC converter product(Integrated FET) which can support the specifications below.
- VIN : DC 48V ~ 57V
- VOUT/IOUT : 12V / 10A
If you have any suitable products, including those…
Part Number: LM70880-Q1 Tool/software: I am looking for an application note that shows how to:
Synchronizing two LM70880-Q1, generating two different voltages, for in-phase operation or for out of phase operation, with one device as master in DRSS mode…
Part Number: LM70880-Q1 Tool/software: Hi
can you advise CONFIG pin connected to AGND or PGND ?
datasheet the picture at page 1 and the picture at Figure 8-8 are different.
Part Number: LM70880-Q1 Tool/software: Hello Texas Instruments Team,
I would like to use the LM70880-Q1 to Convert a 48V Nominal(38V-76V Max) Input to 28V Output.
Can this Device Provide 8A?