Part Number: LM71-Q1 Other Parts Discussed in Thread: LM71 I need formula to convert temperature value especially negative temperature to convert into Hex format as per LM71.
example - how to convert -40degC to Hex value 0xEC03. I have referred the Datasheet…
Part Number: LM71-Q1 Other Parts Discussed in Thread: LM95071-Q1 , LM71 , LM95071 Hello Team,
I just got RFQ about LM71-Q1 from customer.
However when I look over TI.com, I found the LM95071-Q1 which is very similar device. I think LM95071-Q1 is newer device…
Part Number: TMP451-Q1 Other Parts Discussed in Thread: TMP127-Q1 , TMP126-Q1 , LM95071-Q1 , LM71-Q1 Hi, do you have such component but with SPI interface (not I2C)?
Ariel Greenbaum
Part Number: LM95071 Other Parts Discussed in Thread: LM71 , Hello,
Can you confirm if the LM71* and LM95071* devices are "100% compatible" at the software driver level?
I consider adding LM95071* as additional source to the LM71* that we currently…
Other Parts Discussed in Thread: LM71 Hi,
1. I want to measure the temperature of LEDs. I want to place the LM71 next to the LED and want to connect the Pad of the LED with the PAD of the LM71. The PAD of the LED is connected to 5V. Now I want to know…
Part Number: LM71
I could not find in the datasheet or the technical documents anything that would explain to me for sure: is the Exposed Pad in the WSON version of LM71 connected do GND or is it unconnected? I guess any other option would surely be…
Other Parts Discussed in Thread: LM71 Hello,
I currently have an LM71 temperature sensor interfaced with an fpga on my pcb. In looking at the datasheet for the LM71 I was not sure if I should have the fpga drive the SC, spi clk to the temp sensor, for…
Hi Lauren,
I've been looking around, it does not seem we have any code for the STM32 platform since this is not a TI MCU.
The Linux Kernel does include some LM71 drivers, https://www.kernel.org/doc/html/latest/hwmon/lm70.html , which are compatible…
Hi Ren-san,
Thank you for your strong support.
I will refer to "LM71/LM71-Q1 Errata" and inform this information to our customer instead of LM95071 errata. In addition, I will discuss this issue with TI local member.
I greatly appreciate your…
Hi TaeHo,
The only temperature sensor we have that operates between -40C and 150C in a SOT23 package is the LM71 and LM95071 which are both SPI based. Both the LM71 and LM95071 are very similar except the LM95071 has tighter accuracy specs than the LM71…