Part Number: LM73100EVM Tool/software: Hi
Can the IC LM73100 work for a Vin min of 2.5V. We need a overvoltage protection device for our Vin which ranges from 2.5V to 17V.
Can this device be used or is there any other recommended device from TI? Please…
Part Number: LM73100EVM Hi,
I wanted to change the OVP of U2 on LM73100EVM but did not get the result, please help to see what i had missed out for the below 6 steps?
1) Tested the default settings on EVM and is working for OVP=13.76V using R17=191K. …
Part Number: LM73100EVM Other Parts Discussed in Thread: AFE10004EVM Hi
Please provide the CE/EU Declaration of Conformity for LM73100EVM.
The product is CE-marked, however, the CE/EU Declaration of Conformity linked to this part on the T.I website is…
Part Number: LM73100EVM Hi forum members,
I need to connect two power sources in parallel for getting redundancy with two independent power paths. To reach this goal I first thought about simple diodes to put in series to the sources' outputs for oring…
Part Number: LM73100EVM Other Parts Discussed in Thread: TPS2597 HI Team,
What is the current limit for the chip LM73100? Looks like when the In rush current higher than 6 A, the EVM can't turn on.
Best,
Sky
Part Number: LM73100EVM Customer is trying to use LM73100EVM and perform first test with device. They are trying to follow section 5.1 of the user guide but not seeing the output voltage they expect.
Here is what we know about the setup
Power supply connected…
Part Number: LM73100EVM Other Parts Discussed in Thread: TVS2200 Hi
The customer factory found that the LM73100 burned out:
Fail rate: 3/90
The phenomenon of burning is: U59 PIN6 PIN7 PIN9 is short to GND, and the pad has been burned.
There are measured…
Part Number: LM73100EVM Hi I was wondering if someone could tell me if the LM73100EVM board is a two layer board and are there PADS layout files for it ?
Thanx -- Andrew