Part Number: LM73100EVM Other Parts Discussed in Thread: TPS25948 Tool/software: HI
We are working on the laptop design based in the intel alder lake laptop. We are using LM73100RPWR for Type C PD power. The height of this package is around 1mm
We need…
Part Number: LM73100EVM Tool/software: Greetings of the day! I wanted to use this LM73100 IC to control the supply to a solenoid valve. I wanted to know if we can connect the microcontroller to the EN/UVLO pin. Microcontroller VIO=3.3V. Datasheet says, we can…
Part Number: LM73100EVM Tool/software: Hi
Can the IC LM73100 work for a Vin min of 2.5V. We need a overvoltage protection device for our Vin which ranges from 2.5V to 17V.
Can this device be used or is there any other recommended device from TI? Please…
Part Number: LM73100EVM Hi,
I wanted to change the OVP of U2 on LM73100EVM but did not get the result, please help to see what i had missed out for the below 6 steps?
1) Tested the default settings on EVM and is working for OVP=13.76V using R17=191K. …
Part Number: LM73100EVM Other Parts Discussed in Thread: AFE10004EVM Hi
Please provide the CE/EU Declaration of Conformity for LM73100EVM.
The product is CE-marked, however, the CE/EU Declaration of Conformity linked to this part on the T.I website is…
Part Number: LM73100EVM Hi forum members,
I need to connect two power sources in parallel for getting redundancy with two independent power paths. To reach this goal I first thought about simple diodes to put in series to the sources' outputs for oring…
Part Number: LM73100EVM Other Parts Discussed in Thread: TPS2597 HI Team,
What is the current limit for the chip LM73100? Looks like when the In rush current higher than 6 A, the EVM can't turn on.
Best,
Sky
Part Number: LM73100EVM Customer is trying to use LM73100EVM and perform first test with device. They are trying to follow section 5.1 of the user guide but not seeing the output voltage they expect.
Here is what we know about the setup
Power supply connected…