Part Number: LM73605-Q1 We’re starting verification that all semiconductor components LM73605-Q1 have ISO 26262 (Functional safety) according to attached GS95033-1.
Please review and confirm for below parts.
Thanks
Evgeny
Part Number: LM73605-Q1 Hello Team, please could you verify following section in datasheet?
In the datasheet, there’s an error on it : P_IC_Loss(W) must be an subtraction of 2 parts with same Unit. 2nd part is unit [VOLT]!
Many Thanks
Josef
…
Part Number: LM73605-Q1 Hi team,
For LM73605-Q1, can we on line change the working mode from auto mode to FPWM mode during 73605 normal working state? And will it update immediately or we need to toggle EN?
Thanks,
Part Number: LM73605-Q1 Hi Gentlemen,
I need to do the stability simulation of bode plots with different load conditions for LM73605-Q1, but it seems the design tool is still not available in website.
Is there any tools for LM73605-Q1 stability analysis…
Part Number: LM73605-Q1 When the input voltage goes to lower than the output voltage, will LM73605-Q1 have any problem?
This condition means that the input voltage will ramps down or the power supply will be off for some reason before the output capacitor…
Part Number: LM73605-Q1 In the datasheet, the tolerance on the feedback voltage is -1% and +2% - not symmetrical. I would like confirmation because the DC-DC design is failing WCCA.
Part Number: LM73605-Q1 Other Parts Discussed in Thread: LM73605 Hi TI expert,
I am using LM73605 for automotive infotainment LCD panel 3.3V power supply, the LCD panel has a maximum 3.96V input voltage.
During normal operation, will overvoltage happen…
Part Number: LM73605-Q1 Hi team,
I would like to know if there is any limitation in soft-start time or capacitance, such as minimum soft-start time/minimum capacitance (Css).
My customer placed 3.3nF, the typical soft-start time is 1.65ms, but the result…
Part Number: LM73605-Q1 Hi team,
As written in the data sheet of LM73605-Q1: it has over-current protection and thermal shutdown protections.
But our customer wants to know the recovery time of over-current and overheating.
For example, the thermal s…
Part Number: LM73605-Q1 Hi Expert,
I didn't see the detail description about Rsync, could you help to know why need to add Rsync when use external clock ? and why recommend to use 50 to 100 ohm of the terminal resistor?
thanks.
Mark