Part Number: LM73606EVM-5V-400K Tool/software: I wanted to EMI nearfield simulation using this EVB, Can you send me the layout file in ODB++ or .aedt formula?
Part Number: LMR36506-Q1 Tool/software: Hello team,
Customer is going to use LMR36506-Q1, but there is not a corresponding GPN for FSW=400k, Vout=5V work condition, pls check below screenshot, so which one should be used for the case?
Thanks!
Part Number: LM73606EVM-5V-400K Other Parts Discussed in Thread: LM73606
LM73606 - DC/DC, Step Down 1, Non-Isolated Outputs Evaluation Board
Need Country of Origin for this part.
Part Number: LM73606EVM-5V-400K Other Parts Discussed in Thread: LM73606 , Hello,
I plan to use the LM73606 in my next design.
Are the CAD files used for the evaluation module available? I think it was done in Altium. That would be very helpful. …
Part Number: LM73605EVM-5V-2MHZ Hello,
Based on this EVM and using the same schematic, I have designed a board. But the max current rating available without voltage fold back is only 3A. Of course,the layout is not exactly same but the circuit is. Any…
Part Number: LM73605EVM-5V-2MHZ Hello Sir/Madam,
Can you please suggest me the output capacitor and inductor value for 12 to 1.8V output with switching frequency of 2.2Mhz?
Regards, Saikumar
Part Number: LM73606EVM-5V-400K Other Parts Discussed in Thread: LM73606 Tool/software: WEBENCH® Design Tools Hi,
I have bought the LM73606 EVM. and make a loss analysis report. Is there anything about loss analysis you can provide to me?
Thank you
Part Number: LM73605EVM-5V-2MHZ Other Parts Discussed in Thread: LM73605 Hi,
We are planning to use LM73605 in one of our ECU. Before planning to use, we would like to get an EVM for 3.3V output and test it in our lab.
Is it possible to get EVM for…
Hi Robert,
Are you able to scopeshot the L5 inductor current? Place the current loop between L5 and the output capacitance.
If you cannot probe inductor current then the SW node voltage will be OK.
I think the device is hitting current limit, and…