Part Number: LM73606 Hi,
i am using LM73606 in circuit and i know about a technic that i can use DAC to set the output voltage from the DC2DC
how do i connect it?
the output voltage will be 3-12V
the DAC voltage is 0-3.3V
do you have a formula
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606
Hi, TI expert.
A customer company constructed a circuit using the LM73606-Q1, and I have a few questions regarding it.
-INPUT: 5V, OUTPUT 4V
(Questions)
1. Fsw: Use 500KHz (Is Fsw suitable…
Part Number: LM73606 Hi TI experts,
I use LM73606 for automotive application. Due to the safety concern, does LM73606 have Vout voltage protection if Vout over or under (+10%)
Ex: Vout 3.3V
thanks
Smith
Part Number: LM73605-Q1 Other Parts Discussed in Thread: LM73606 , LM73605 Hi, the LM73605 & LM73606 are parts from the same family. Also they share a datasheet. The only difference what I see is, that the current limitation is different. Is for both…
Part Number: LM73606 Other Parts Discussed in Thread: LMR33640 Hi Sir,
May I know LM73606 can support 12V convert to negative 5V capability? if yes, please help us to provide reference schematic, thanks!
Part Number: LM73606
Figures 65-68 of the datasheet appear to show a delay (approximately 800 us) between the EN pin going high and the start of the ramp on the output (see image below). However, the Soft Start timing characteristics in section 6.6 of…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606 A customer company constructed a circuit using the LM73606-Q1, and I have a few questions regarding it.
-INPUT: 5V, OUTPUT 4V , 6A
In the attached circuit diagram, I used 4.7uH of the inductor…
Part Number: LM73606EVM-5V-400K Other Parts Discussed in Thread: LM73606LM73606 - DC/DC, Step Down 1, Non-Isolated Outputs Evaluation Board
Need Country of Origin for this part.
Part Number: LM73606 Hi, TI expert.
Will there be any risk of damage to LM73606 after long time use in Dropout? (datasheet Figure 56. VIN=11V~12V VOU=12V)