Part Number: LM73606-Q1 Hello
I would like to know which part number called for RNP0030A and RNP0030C package?
- LM73606Q RNPTQ1
- LM73606QU RNPTQ1
WQFN (30) Wettable and nonwettable flanks
Wettable flanks is the RNP0030A package if I understand corre…
Part Number: LM73606-Q1 Hi team,
My customer is evaluating LM73606-Q1 loop stability over temperature.
Left hand side is room temp, Right hand side is Hot temp. The room temp result is no problem ,but for hot temp, the phase value between 500Hz to 1kHz…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606
Hi, TI expert.
A customer company constructed a circuit using the LM73606-Q1, and I have a few questions regarding it.
-INPUT: 5V, OUTPUT 4V
(Questions)
1. Fsw: Use 500KHz (Is Fsw suitable…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606 A customer company constructed a circuit using the LM73606-Q1, and I have a few questions regarding it.
-INPUT: 5V, OUTPUT 4V , 6A
In the attached circuit diagram, I used 4.7uH of the inductor…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: TPS7B68-Q1 , , LM73605 Hi, TI expert
7V DC-DC (LM73606-Q1) + 5V LDO (TPS7B68-Q1) We ask about the problem of output voltage when input power fluctuates.
The contents of the inquiry are as follows…
Part Number: LM73605-Q1 Other Parts Discussed in Thread: LM73606 , LM73605 Hi, the LM73605 & LM73606 are parts from the same family. Also they share a datasheet. The only difference what I see is, that the current limitation is different. Is for both…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606 We are looking in confirmation of the circuit correctness which is requested by seniors. Kindly do the needful if anymore information required to confirm please free to ask.
Input supply…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73605 Hi TI,
I want to know the behavior for SYNC/MODE pin of LM73606 .
I see that I can use MODE pin to select auto or FPWM mode. Can I change the mode while power supply is operating? For example…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606 , LMZ23608 HI Team.
Can the two output terminals of LM73606 be directly connected in parallel to improve the current output capability?