Part Number: LM74502-Q1 Other Parts Discussed in Thread: LM74502 Dear TI Representative, We are currently considering the adoption of the LM74502 for reverse protection applications, and we would appreciate it if you could kindly provide us with your…
Part Number: LM74502 Hi Team,
I've wired a LM74502 as a load switch and setup the EN pin with RC circuit for a delay enable using techniques describled at www.ti.com/.../slvaea3.pdf
But when I measure the vout, it was instantly available when I connected…
Part Number: LM74502 Other Parts Discussed in Thread: TPS26750 Hi dear,
I couldn't understand why the R112 and C7 components connect the SRC pin of the LM74502 IC in this reference design? In datasheet of LM74502 this type of connection use for the…
Part Number: LM74502-Q1 Other Parts Discussed in Thread: LM74502 Hi Team,
There's a question about the LM74502 that needs confirmation. The LM74502 drives the external MOSFETs via a CP (Concurrent Controller). Currently, the customer has about 12 external…
Part Number: LM74502-Q1 hi expert
This is my schematic diagram.
This is my schematic diagram. Please help to check it. The current situation is that 6V can start normally, but 5V cannot start properly.
Part Number: LM74502 Tool/software: Hello,
I would like to use the surge stopper application shown in the datasheet. In my case, I also need to handle negative surge impulses. For this reason, I am using two Z-diodes with a clamping voltage of 62 V…
Part Number: LM74502-Q1 Other Parts Discussed in Thread: LM74502 Hi team,
For the LM74502-Q1 undergoing an E-10 test, if the input VIN is shorted to GND, the LM74502-Q1 needs to quickly turn off its internal FET. How long does this shutdown…
Part Number: LM74502-Q1 Other Parts Discussed in Thread: LM74502 , LM74800-Q1 , TPS4800-Q1 Tool/software: Hello,
I'm looking at the LM74502 for a reverse input protection with load turn-off. Looking at the package and suggested footprint, it seems like…
Part Number: LM74502 Hello,
I am hoping to use the LM74502 in the following setup: My question is, when the input is at a lower voltage then the output, and the MCU has the LM74502 enable pin pulled low, will there be any leakage from VOUT to VIN? If…