Part Number: LM74502H-Q1 Tool/software: I am using LM74502H-Q1 to drive a AONS66920 MOSFET to have overvoltage protection to the circuit afterwards. Can I use the charge pump output of the same IC to switch another AONS66920 MOSFET somewhere else in the…
Part Number: LM74502H-Q1 Other Parts Discussed in Thread: LM74800-Q1 Tool/software: Hi,
In a specific motor drive related automotive application, I need back-to-back MoSFET to prevent back EMF when battery supply to the drive is disconnected. Please…
Part Number: LM74502H-Q1 Other Parts Discussed in Thread: LM74703-Q1 , INA230 , INA300 , LM5148-Q1 , LM74910H-Q1 , LM74900Q1EVM Tool/software: Hi,
I’m designing an ECU PCB that will operate from a 48 V vehicle supply and must include input protection…
Part Number: LM74502H-Q1 Tool/software: Hi team,
Can LM74502H-Q1 tolerate 70V max rating? Customer wants to use it in 48V system. Thanks.
Best Regards
Grey
Part Number: LM74502H-Q1 Tool/software: I designed my circuit to lock out at 4V and start up at 6V when connected to Vin it works perfectly but it failed when I ran ISO 7637-2 pulse 1 since the pin can only handle -60V.
I'm wanting to connect it to…
Part Number: LM74502H-Q1 Tool/software: Hi Team,
We are planning to use LM74502H-Q1 in one of our applications.
We will be controlling two different circuits of back-to-back N-channel FETs.
So we can not connect the common Source of back-to-back…
Part Number: LM74502H-Q1 Tool/software:
Hello TI Team,
I am evaluating an existing protection circuit that uses the LM74502HQDDFRQ1. the circuit is attached .
Protection circuit.pdf
I would like to know if I might encounter issues when testing…
Part Number: LM74502H-Q1 Other Parts Discussed in Thread: LM74502H Tool/software: Hi Team,
We are planning to use LM74502H in one of our applications. Please address the queries below.
1. What are the minimum and maximum voltage levels at the gate…
Part Number: LM74502H-Q1 Other Parts Discussed in Thread: LM74502H Tool/software: Hello TI Team,
I am using the LM74502H-Q1 as a protection controller configured as a high-side switch with undervoltage, overvoltage, and reverse polarity protection.…