Norbert,
Another part you may want to check out is the LM74610-Q1. It has zero quiescent current and would work well in your application with a lower cost compared to the solution you are considering.
Mathew
Hi Satoshi,
for Idea diode behavior, you can also look at SM74611 that has an integrated FET.
for external FET implementation, please have a look at LM74610-Q1
Regards, GJ
Vince,
SM74611 can provide a very efficient low cost reverse polarity solution. However in terms of it's capability to be used in a full bridge rectifier lacks because the absence of gate pull down when a reverse polarity occurs. The speed at which the…
Part Number: LM74700-Q1 Hello,
What's the Production Release schedule and volume availability of this part? I would like to use this part in my design for which we would be going to PCB Layout in a couple of weeks. And, prototyping in couple of months…
MiHai,
Does your customer require Q100 parts ?
If so, your options are the LM5060-Q1, LM74610, and the LM5050-Q1. There are apps for both these parts to provide protection in a ISO 7637 Environment. The particulars of the customer application will determine…
Part Number: PMP22504 Tool/software: Dear team,
My customer would like to develop DC rectifier.
- Input : +-6V
- output current : 1A
Can I promote PMP22504 design? If yes, How can I modify PMP22504 to fit customer specification?
If not, Would you recommend…