Part Number: LM74700-Q1 Tool/software: Hi,
We are using LM74700QDBVRQ1- Automotive ideal diode controller. and IPB120N06S4 ( Infineon N-MOSFET) is used as controller mosfet which has VGS(th) = 4V(max).
Please provide us a confirmation whether this…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74800-Q1 , LM74502-Q1 Tool/software: Hello TI Team
In my application I need to quickly disable the external FET in case of overload. Can I use an external bipolar transistor to short circuit…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74502-Q1 , LM74800-Q1 , LM74720-Q1 Whether LM74700-Q1 could support Hot-Plug?
If not, whether we have other product which could support hot-plug?
Part Number: LM74700-Q1 Hi E2E team,
From the LM74700-Q1 datasheet 10.1.1.2.2 MOSFET Selection:
It shows the VGS rating is 15-V:
This would include any anticipated fault conditions. It is recommended to use MOSFETs with voltage rating up to 60-V…
Part Number: LM74700-Q1 Good morning, I'm considering to use the IC LM74700-Q1 in order to protect our battery-operated devices against accidental polarity reversal. Our device use 12Vdc battery, voltage can vary from 14 to 10 Vdc. The nominal current…
Part Number: LM74700-Q1 According to LM74700-Q1 datasheet, the device enters reverse current protection mode when Vanode - Vcathode < -11mV. I assume the external N MOSFET is turned off in this mode, hence Vanode - Vcathode will no longer be < -11mV.…
Part Number: LM74700-Q1 HI TI TEAM
I have various 54V/14.8A models and using LM74700QDBVRQ1
When OVP occurs, although there is a protection circuit, due to the problem of response speed, the OVP voltage will exceed 65V, exceeding the maximum voltage…
Part Number: LM74700-Q1 Hi team,
In datasheet, T_Reverse delay is defined Typ.0.45us/Max0.75us. Can customer estimate this time on their use case?
Regards,
Youhei MIYAOKA