Part Number: LM74700D-Q1 Hello,
As per Datasheet, the recommended condition is upto 65V, but still wanted to check if working at higher limits and not at standard 48V, does it have any design limitations.
My project is to replace diode for selecting…
Part Number: LM74700D-Q1
Tool/software:
hello,
i test the lm4700 and csd18511 for our configuration and design an prototype. everything works as excepted.
but this is my second try so i want to be sure that everything complied with.
We use the…
Part Number: LM74700D-Q1 Other Parts Discussed in Thread: LM74681 Hi,
Are there any solutions that support an input voltage VIN +/- 60V , where a bridge rectifier is used at the back end to convert the output to positive DC? Note that the input source…
Part Number: LM74700D-Q1 Tool/software: Can one LM74700D-Q1 drive two or more parallel-connected MOSFETs?
On/off delays due to increased MOSFET Ciss are not an issue.
During forward regulation mode,the ANODE to CATHODE voltage is regulated to…
Part Number: LM74700D-Q1 Other Parts Discussed in Thread: TVS5800 Hi TI,
Are there any guidelines or reference designs for power-protection design in automotive 48 V battery systems?
I need to protect electronics powered from a 48 V battery, which…
Part Number: LM74700D-Q1 Other Parts Discussed in Thread: LM74500-Q1 Tool/software: Dear team,
Is there any way to use LM74700D-Q1 for only RPP circuit? The background of this query is because we are looking for 48V automotive ideal diodes which only…
Part Number: LM74700D-Q1 Other Parts Discussed in Thread: TIGER Tool/software: Hi,
If EN will high and Anode is low (no input), is there any concern?
According to datasheet, the gate driver should be still in OFF state.
Thanks and Best regards…
Part Number: LM74700D-Q1 Tool/software: Hi,
I'm looking to use the LM74700D-Q1 in in a 24V automotive system to protect the rest of my system against reverse battery connections.
In the LM74700D-Q1 datasheet, section 10.2.4 "Selection of TVS Diodes…
Part Number: LM74700D-Q1 Tool/software: Hello,
My client is looking for an ORing controller solution that supports the following conditions:
- ORing of two 12V Power Rails
- Max VIN : 18V or higher
- IOUT: 2.5A or higher
- The lower the Rds…