Part Number: LM74701-Q1 Hello,
A customer wants to know a bit more details of the datasheet explanation.
In 9.2.2.2 MOSFET Selection of the datasheet, I think there are 2 estimations as listed below. Would you please explain a bit more details about…
Part Number: LM74701-Q1 Hello,
I've tested the LM74701-Q1 with 2 power supplies of 54V and 2 N-Mosfet (IAUZ40N06S5N050ATMA1) with Vds:60V, Id: 40A, Rds On: 5mOhm, Vgs: -20V;+20V, Qg: 23.5 nC
I've connected pin EN to the ANODE and left SW pin floating…
Part Number: LM74701-Q1 Other Parts Discussed in Thread: LM74800-Q1 Hi Sirs, My customer is interested in the TVS-less ideal diode device LM74701-Q1 and has a question about the compliance test result. Could it pass the SAE J1455 test and SAE J1113-11…
Part Number: LM74701-Q1 Other Parts Discussed in Thread: LM74700-EP , LM74700-Q1 , Hi Team,
1.May I know the deference with LM74701-Q1 & LM74700-Q1 & LM74700-EP?
2.Please help provide comparison table ,THX
Part Number: LM74701-Q1 Hi Team,
Our customer would like to know when will the LM74701 (PLM74701QDDFRQ1) be qualified and when it will be available for production.
Regards,
Danilo
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: LM74701-Q1 Tool/software: Upon trying to run the simulation of the built-in TI circuitry LM74701-Q1, this error appears.
PSpice for TI was freshly installed with the ADMIN account of the PC…
Other Parts Discussed in Thread: LM74701-Q1 Dear Team,
We are using LM74701QDDFRQ1 &TMP236AQDBZTQ1 in our ASIL-D compliance product.
As the mentioned components are not ASIL qualified, I need to do component evaluation to use it in safety application…
Part Number: LM74501-Q1 Other Parts Discussed in Thread: LM74700-Q1 , , LM74701-Q1 Hi team,
there is a question I want to consult you. if LM74501-Q1 have no TVS less function, like the device LM74700-Q1, we should add TVS at where to pass the ISO7637…
Hi Rajkumar,
Since you asked for a TVS-less controller, I recommended LM74701-Q1 and LM74721-Q1.
You can use LM74700-Q1 as well but will need an extra TVS.
To replace LM74721-Q1, you can use LM74800-Q1.
LM74502-Q1 can't be used since it does not…
Part Number: LM74704-Q1 Other Parts Discussed in Thread: LM74703-Q1 , LM74701-Q1 Tool/software: Hello Expert,
Could you please answer following questions?
Does EC table's FET GOOD HIGH include voltage drop at RFETGOOD or we should add voltage drop…