Part Number: LM74720-Q1 Tool/software: Hi team,
if customer doesn't use SW pin, can they leave if floating? or must connect SW to VSNS?
Thanks
Scarlett
Part Number: LM74720-Q1 Tool/software: Hi team,
I have a question about an operating condition of boost converter in LM74720-Q1.
Below is from datasheet page 10, functional block diagram.
You can see Voltage on "C" pin is compared against 2.5V threshold…
Part Number: LM74720-Q1 Tool/software: Hi team,
May I know the feature of load dump protection detailed? I found that adjustable over voltage cut-off protection is one of the feature of load dump protection. Any other features related to load dump protection…
Part Number: LM74720-Q1 Tool/software: Dear TI team,
We are considering using this IC in an overvoltage protection circuit for the input of a control circuit.
However, we would like to stop the circuit by detecting the overvoltage with a uC while protecting…
Part Number: LM74720-Q1 Tool/software: Hi My input voltage is 6V to 18V and load current is 20A, So what is the possible voltage across Cdvdt capacitor during normal operation and during turn off of Q2 MOSFET. This is to ensure the capacitor voltage rating…
Part Number: LM74720-Q1 Tool/software: Hi team,
Could you please have a look on following question:
"
Vsns is connected to Pin-12 C, can this circuit work normally? please help us confirm it. thanks very much!
"
Best
Part Number: LM74720-Q1 Tool/software: Hi TI,
In my custom board, Two inputs are received from two external battery power supplies, 28V each. I need to implement Oring circuit, where these 2 battery power supplies are given to an ORing circuit (LM74720…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM7481-Q1 , LM7480-Q1 , , LM74721-Q1 , LM74720-Q1 , LM74502-Q1 , LM74900 , LM74910-Q1 Tool/software: Hi TI Team,
I am looking for an ideal diode controller/ideal diode with the below specs.
- Input voltage…
Part Number: LM74720-Q1 Other Parts Discussed in Thread: LM74502-Q1 , LM74800-Q1 Hi Team,
I'd like to ask you about external back-to-back FET circuit of LM74720. There is no application material for this circuit on TI website. Please let me know how to…