Part Number: LM74721-Q1 Hi team,
The datasheet shows a recommended L1 = 100uH, but I would like to know the min and max values for L1. For example, please let me know what phenomena could occur if this is changed to 47uH or 200uH.
Regards,
Haya…
Part Number: LM74721-Q1 Hi team,
When driving back to back FET, the total system Iq will be the spec written in the datasheet, correct?
Also what does I(PD_SRC):pullup current mean? Is it a drive current to FET?
Regards,
Hayashi
Part Number: LM74721-Q1 Other Parts Discussed in Thread: LM5050-1 Hi Team,
my customer is looking for a ideal diode controller that starts up at 3.3V at all conditions. The classic LM74700 mentiones 3.2V but that is only during operation. At startup…
Part Number: LM74721-Q1 Tool/software: Hello team,
My customer want to double confirm the RTN usage for LM74721-Q1.
1. If they connected RTN to the GND, reverse polarity is disabled, whether reverse current blocking is also disabled?
2. Would you…
Part Number: LM74721-Q1 Other Parts Discussed in Thread: LM74800-Q1 Tool/software: Hi Expert,
This is a question about the LM74800-Q1 that was raised on the agenda in the previous thread.
Is the device tolerant to tests such as overvoltage required…
Part Number: LM74721-Q1 Other Parts Discussed in Thread: LM74800-Q1 Tool/software: Hello Expert,
Could you please clarify about device's voltage rating during reverse voltage connection?
This device's A to GND minimum voltage rating is "-(VCLAMP+1…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM7481-Q1 , LM7480-Q1 , , LM74721-Q1 , LM74720-Q1 , LM74502-Q1 , LM74900 , LM74910-Q1 Tool/software: Hi TI Team,
I am looking for an ideal diode controller/ideal diode with the below specs.
…
Part Number: LM74721-Q1 Hello,
Is it possible to remove the ideal diode FET and connecting the anode and cathode together and only using the load disconnect as a load switch?
Cheers,
K
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM74721-Q1 , LM74720-Q1 Hello, can you tell me the LM74722-Q1,LM74721-Q1,LM74720-Q1 when released?
Hi Rajkumar,
Since you asked for a TVS-less controller, I recommended LM74701-Q1 and LM74721-Q1.
You can use LM74700-Q1 as well but will need an extra TVS.
To replace LM74721-Q1, you can use LM74800-Q1.
LM74502-Q1 can't be used since it does not…