Part Number: LM74722-Q1 Other Parts Discussed in Thread: TPS3760 Tool/software: Hi teams,
Please help to check it ,many thanks!
solution: LM74722+TPS3760
test item:slow rise
description: when the voltage of KL30_VBAT1 rise to 5.61V, the voltage of KL30_VBAT1…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM74502-Q1 Tool/software: Hi everybody,
I'm looking for a high side gate driver for my system: the component should be able to open a MOS whenever a sensed voltage overcomes 20V (in the LM74722…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM7481-Q1 , LM7480-Q1 , , LM74721-Q1 , LM74720-Q1 , LM74502-Q1 , LM74900 , LM74910-Q1 Tool/software: Hi TI Team,
I am looking for an ideal diode controller/ideal diode with the below specs.
- Input voltage…
Part Number: LM74722-Q1 Hi Team
do we have any replacement for LM74722-Q1? customer can't use this application due to high I sleep(they need below 100uA).
Their operating voltage is 6~18V so the resistor is too smaller.
they need 14V 1A solution…
Part Number: LM74722-Q1 Tool/software: Hello, I am Makoto.
Datasheet says,
The SMBJ33CA TVS diode can be used for 12-V battery protection application. The breakdown voltage of 36.7 V meets the jump start, load dump requirements on the positive side and…
Hi Rudraprasad,
Firstly we should understand the root cause of LM74722-Q1 failure.
When the down-stream circuit HSD device turns OFF the power path after detecting a output short, there can be be transient over voltage seen at the input of HSD which is…
Part Number: LM74722-Q1 Hello,
I am trying to simulate the ISO 7637-2 pulse 1.
Why Vin is fluctuating if i consider load as around 20A.
If i take load around 50mA, then Vin is not fluctuating.
What is the reason behind this problem.
Part Number: LM74722-Q1 Hello,
How to choose the external components. The minimum value shown is the typical value of the component?
For example, let's say i have 1uF at C and it will have 10% tolerance and also due to temperature effect the value will…