Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM74800-Q1 , Hi,
Today I'm using the LM74800-Q1/LM74801-Q1 in my product.
Since those components aren't in the stock I want to replace them with the LM74722-Q1.
Since the LM74800-Q1/LM74801-Q1…
Part Number: LM74722-Q1 I'm currently checking if the component could be used in my application.
However I do have little concerns regarding conducted / radiated emssions caused by the boost regulater implemented in the component..
Unfortunately the…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM7472EVM , LM74720-Q1 , LM74502H-Q1 , LM74502H Hi Expert,
Our customer is looking for device replacing AUIR3242S. Actually I provide LM7472EVM to them for testing. They use our EVM to drive 6pcs NVMTS0D6N04C…
Part Number: LM74722-Q1
Hi team,
Regarding LM74722-Q1 -
If OV pin is not used, how should I connect this pin? Can I connect it to ground via a pull-down resistor and what is the recommended pull-down resistor?
Regarding Zener usage, if the selected MOSFET…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: BQ34Z100-G1 , LM5060-Q1 Hello Team,
We are designing a BMS around the BQ34Z100-G1. The battery specs are max 54.6V and 6A. We want to implement a high side switch for the power rails and…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM74700-Q1 Hi Expert,
Our customer plan to use LM74722-Q1 to drive 6pcs IAUC120N06S5N017. How to calculate the turn on time? May I know the source current of GATE pin?
And why Zener diode is only…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM74721-Q1 , LM74720-Q1 Hello, can you tell me the LM74722-Q1,LM74721-Q1,LM74720-Q1 when released?
Hi Eric,
Good to know that you are able to reproduce the issue on standalone LM74722-Q1 circuit.
From your description, I can understand that the device fails when the Enable pin is connected to input probably because of glitches on EN (ON and OFF the…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74720-Q1 Hi Team,
1. The lm74700 has an external single MOS, and the datasheet has a shutdown current of 1uA (EN = low level), but when the 74700 single MOS is external, even if it is turned off…
Part Number: LM74722-Q1 Hi Team,
May I know the gate pin peak source current of LM74722-Q1? Our customer will use total 4 MOSFET to conduct total 420A current, the source capacity will guide us the rough turn on time of MOSFET. Thanks.