Part Number: LM7480-Q1 Hi,
Please teach me the replacement parts of BZG03B62-M which is written in "10.3.2.3 VS Capacitance, Resistor and Zener Clamp" of the datasheet. (without Vishay )
Regards, PAN-M
Part Number: LM7480-Q1 Hello!
I have used the LM74801QDRRRQ1 in the input power stage of a new product I am currently developing (see attached screenshot for circuit details).
The idea is to have a fixed in-rush current limiter path through R1 and…
Part Number: LM7480-Q1 It always constitutes an ideal diode of on-circuit.
When the power is turned on and the standing waveform is checked, the Vg-s voltage is determined at 3.6V.
It becomes 0V momentarily, and 8V is output.
Since it is always…
Part Number: LM7480-Q1 Hello,
Are there any concerns or considerations that should be used when paralleling MOSFETs on the LM74801QDRRRQ1, when used in the ideal diode configuration below (Q1 would be 2 parallel instances of Infineon IPT007N06N). Load…
Part Number: LM7480-Q1 Hello,
If I want to totally disconnect the device (i.e. because even 2.87uA nominal shutdown / quiescent current is too much for us over temperature and tolerance):
Is there a way I can do that using discrete MOSFETs? Would…
Part Number: LM7480-Q1 Other Parts Discussed in Thread: LM74800-Q1 Team,
Do we have Spice model of LM74800-Q1?(Not PSPICE, we would like to do the WCCA test) Could you help send it via email? Thank you.
roy.chou@ti.com
Regards, Roy
Part Number: LM7480-Q1 Hi team ,
Per application note, LM7480-Q1 gate drive strength can be extended to charge pump capacity(~3mA) with below configuration:
Customer would like to know whether there's other external circuit configuration which could…