Part Number: LM7481-Q1 Other Parts Discussed in Thread: LM74900-Q1 , LM7481 Tool/software: Hello Team,
am using the LM7481-Q1 in my design and would appreciate your guidance on setting the current limit.
As per the datasheet, the LM7481-Q1 supports…
Part Number: LM7481-Q1 Hi Teams,
The resistor values on the EN/UVLO pin are:
Upper resistor: 34.8 k
Lower resistor: 8.06 k
Based on our calculation, we expect VBAT0 to shut down at approximately 6.1 V (EN/UVLO falling threshold: 1.091 V to…
Part Number: LM7481-Q1 Is there any particular reason why the battery monitor ratio is chosen to be 8:1 in the LM7481-Q1 datasheet? Is it desirable to increase the ratio as ones over voltage threshold increases?
Part Number: LM7481-Q1 Other Parts Discussed in Thread: LM7480 Hi Team
Our product incorporates the LM74810-Q1 for protection
The configuration parameters are outlined below:
- Input Voltage (Vin): 22 to 27 and 24V nominlal
Please find the attached…
Part Number: LM7481-Q1 Tool/software: Hi Teams,
We add choke L2204 for EMI as following schematic but find that Vout is no output.
What might be the reason for this issue? Thanks.
Part Number: LM7481-Q1 Other Parts Discussed in Thread: LM7481 Tool/software:
Hello ,team
there is a requirement about the redundant supply from customer , can i just copy the LM7481 circuit and connect like below ? is there any risk if the VIN1 and…
Part Number: LM7481-Q1
I want to use R_VAR to achieve a constant power load of 1 60W. However, I get this error during the simulation. Can you help me figure out why? The attachment is my project file. LM74810-Q1_PSPICE_TRANS.zip
Part Number: LM7481-Q1 Tool/software: We need to quickly turn off the Q1MOS tube of LM74810 after detecting a certain trigger signal. I would like to ask if our following design is OK. If not, please tell us where the problem lies and give a recommended…
Part Number: LM7481-Q1 Other Parts Discussed in Thread: LM7481 Tool/software: Hi, we are Using LM7481 - Q1 in our design; We need spice model and reference design Schematic and Simulation design
Part Number: LM7481-Q1
want to use VCCS to achieve a constant power load of 1 60W. However, I get this error during the simulation. Can you help me figure out why? The attachment is my project file. LM74810-Q1_PSPICE_TRANS.zip