Part Number: LM7481-Q1 Other Parts Discussed in Thread: LM7481 , LM5050-1 I have an application in which I need a MOSFET-based ideal diode circiut that can operate with input voltages down to close to zero volts, by powering the controller from a separate…
Part Number: LM7481-Q1 Tool/software: Hi team,
I see in LM74810 datasheet, it states that the absolute maximum rating between OUT to GND is -0.3~70V, so inside the LM74810 chip, there is a diode connected in reverse direction between OUT pin and GND…
Part Number: LM7481-Q1 Tool/software: For the LM74810QDRRRQ1 component under UV conditions, should the parameter used be the RISING value of 1.231 or the FALLING value of 1.132? The requirement is UV: 6.5V, OV: 18.1V.
Below is our calculation method;…
Part Number: LM7481-Q1 Tool/software: Hi team,
The customer found that in this post we recommended the customer to use this tool. I would like to confirm with you whether TI recognizes the authenticity and reliability of this tool. If it is authentic…
Part Number: LM7481-Q1 Tool/software: Hello Expert:
We are currently evaluate LM74810-Q1 controller current consumption ( quiescent current of this controller in normal operating mode)
(1)I saw the controller define total system quiescent current…
Part Number: LM7481-Q1 Other Parts Discussed in Thread: LM7481 Tool/software: Hello TI experts,
I'm trying to simulate LM7481-Q1 in PSpice for TI,
I downloaded the LM74810-Q1 PSPICE Transient Model from the component page. Link to the component page…
Part Number: LM74722-Q1 Other Parts Discussed in Thread: LM7481-Q1 , LM7480-Q1 , , LM74721-Q1 , LM74720-Q1 , LM74502-Q1 , LM74900 , LM74910-Q1 Tool/software: Hi TI Team,
I am looking for an ideal diode controller/ideal diode with the below specs.
…
Part Number: LM7481-Q1 Tool/software: Hi,
Our design is a PCIe gen4 add-in card with 12V input supply. The max current on the rail is about ~11A.
Since the power is >100W, we will have an auxiliary power connector to supply the additional power. …