Hi Shiven,
Any ideas for questions above:
1. Is the different behavior due to differences in EMVs (e.g. layout)?
2. Or is the linear operation bandwidth different in these devices ( LM74912-Q1 vs. LM74720)?
3. What is the bandwidth of linear operation…
Part Number: LM74912-Q1 Other Parts Discussed in Thread: LM74912 Tool/software: Hi all,
8.3.5 Low IQ SLEEP Mode (SLEEP, SLEEP_OV)
in the manual.
’’As an additional layer of protection, device also features thermal shutdown with latch off feature…
Part Number: LM74912-Q1 Other Parts Discussed in Thread: LM74912Q1EVM , Tool/software: Dear Sir/Madam,
I made some modification to the LM74912Q1EVM to drive a motor. The modifications are: C5 changed to 100nF C10 removed R12 changed to 0R J5 removed…
Part Number: LM74912-Q1 Other Parts Discussed in Thread: LM74912 Tool/software: Hello,
I am designing a board with two LM74912 controllers in an O-Ring configuration to power a single board from two batteries.
The system is intended to remain in sleep…
Part Number: LM74912-Q1 Other Parts Discussed in Thread: LM74930-Q1 Tool/software: Dear Sir/Madam, Sorry for the similar questions I have been asking based on LM74810-Q1, LM74930-Q1 and now LM74912-Q1. Just trying to avoid a re-spin. Look like the LM74912…
Part Number: LM74912-Q1 Tool/software: Dear Sir/Madam, I have a couple of questions.
(1) SLEEPn If not used can the SLEEPn pin be connected directly to VS without current limit resistor? The datasheet page 3. >> When not used, should be tied to EN or…
Part Number: LM74912-Q1 Other Parts Discussed in Thread: LM74912 Tool/software: I've downloaded LM74912-Q1 PSpice Transient model (snom786.zip) and I'm trying to simulate the example design included with the model (LM74912-Q1 STARTUP SIMULATION). The…
Part Number: LM74912-Q1 Tool/software: Hi team,
It seems like the switching speed of DGATE pin is much faster than the switching speed of HGATE pin. Why are there differences between the switching speed of DGATE pin and HGATE pin?
Best regards,…